REGEN.TEMP

Description

This parameter returns the measured temperature of the power module for the regen resistor.

Versions

Action

Version

Notes

Implemented

02-07-03-000

General Information

Type

Read Only

Units

Deg C

Range

N/A

Default Value

N/A

Data Type

Float
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
REGEN.TEMP

3007h

0bh

Signed32

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.TEMP

2410

96A

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.TEMP

2410

Float

Read Only

-